Installation - Facility Explorer - Part No. 24-10143-616 - Field Device - PCA: Advanced Application Programmable Controller

FX-PCA3611 Advanced Application Programmable Controller Installation Instructions

Product
Controls > Programmable Controls > PCA: Advanced Application Programmable Controller
Document type
Installation Guide
Document number
Part No. 24-10143-616
Document revision
D
Revision date
2019-03-22

Observe the following guidelines when installing an FX-PCA3611:

  • To minimize vibration and shock damage, transport the controller in the original container.

  • Verify that all parts shipped with the controller.

  • Do not drop the controller or subject it to physical shock.