Network Port - Facility Explorer - LIT-12013492 - FX-PCA2513-0 - FX-PCA3613-0 - FX-PCA25 Advanced Application Programmable Controller - FX-PCA36 Advanced Application Programmable Controller

FX-PCA2513 and FX-PCA3613 Protocol Implementation Conformance Statement

Brand
Facility Explorer
Product name
FX-PCA25 Advanced Application Programmable Controller
FX-PCA36 Advanced Application Programmable Controller
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013492
Revision date
2020-11-11
Language
English

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Network Port

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

APDU_LENGTH X   399 X 128 to 65,535
CHANGES_PENDING X 416
LINK_SPEED X 420
NETWORK_NUMBER X   425 X 0 to 65,534
NETWORK_NUMBER_QUALITY X   426
NETWORK_TYPE X 427
OBJECT_NAME X 77
OUT_OF_SERVICE X 81
PROTOCOL_LEVEL X 482
RELIABILITY X 103
STATUS_FLAGS X 111
BACNET_COMMAND X 417 X
BACNET_MAC_ADDRESS X 423 X
DESCRIPTION X 28 X
LINK_SPEED_AUTONEGOTIATE X 422
MAX_INFO_FRAMES X 63 X 1 to 255
MAX_MASTER X 64 X 4 to 127
ACTIVE_BAUD_RATE X 2861 Enumerated
ALARM_STATE X 1006 Enumerated
CLEAR_STATISTICS X 2427 Boolean X
ENABLED X 673 Boolean X
EXECUTION_PRIORITY X 2197 Enumerated X
ITEM_REFERENCE X 32527 Character String
JCI_NPO_APDU_RETRIES X 1851 Byte X 2 to 10
JCI_NPO_APDU_SEGMENT_TIMEOUT X 1849 Unsigned Integer X 1,000 to 65,535
JCI_NPO_APDU_TIMEOUT X 1850 Unsigned Integer X 1,000 to 65,535
JCI_NPO_CHANGES_PENDING_BITSTRING X 1852 Byte
JCI_NPO_PORT_TYPE X 1848 Enumerated
LATCH_STATISTICS X 2426 Boolean X
MULTICAST_RESPONDER X 30095 Byte X
OBJECT_CATEGORY X 908 Enumerated X
PORT_STATUS X 2866 Enumerated
PROT_ENG_OUT_RESOURCE X 2020 Unsigned
REPLY_TIMEOUT X 2865 Unsigned
SOFTWARE_ADDRESSING_ENABLED X 2863 Boolean
STATUS X 512 Enumerated
USAGE_TIMEOUT X 2864 Byte
USER_NAME X 2390 Character String