Standard Object Types Supported - Facility Explorer - LIT-12013492 - FX-PCA3613-0 - FX-PCA2513-0 - FX-PCA36 Advanced Application Programmable Controller - FX-PCA25 Advanced Application Programmable Controller

FX-PCA2513 and FX-PCA3613 Protocol Implementation Conformance Statement

Product
Controls > Programmable Controls > FX-PCA36 Advanced Application Programmable Controller
Controls > Programmable Controls > FX-PCA25 Advanced Application Programmable Controller
Document number
LIT-12013492
Revision date
2020-11-11

The following is a list of the standard object types as defined by ASHRAE that are currently supported in this product. See the section of the supported object type for details.

  • Accumulator

  • Analog Input

  • Analog Output

  • Analog Value

  • Binary Input

  • Binary Output

  • Binary Value

  • Calendar

  • Device

  • Event Log

  • File

  • Multistate Value

  • Network Port

  • Notification Class

  • Schedule

  • Trend Log