Character Sets Supported - Facility Explorer - LIT-12013492 - FX-PCA3613-0 - FX-PCA2513-0 - FX-PCA36 Advanced Application Programmable Controller - FX-PCA25 Advanced Application Programmable Controller

FX-PCA2513 and FX-PCA3613 Protocol Implementation Conformance Statement

Product
Controls > Programmable Controls > FX-PCA36 Advanced Application Programmable Controller
Controls > Programmable Controls > FX-PCA25 Advanced Application Programmable Controller
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013492
Revision date
2020-11-11

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

IBM®/Microsoft® Double-Byte Character Set (DBCS)

ISO 10646 Universal Character Set-2 (UCS-2)

ISO 10646 (UCS-4)

ISO10646 (UTF-8)

ISO 8859-1

Japanese Industrial Standard (JIS) X 0208