Accessories - Facility Explorer - LIT-1900687 - Field Device

FX-ATV Handheld VAV Box Balancing Tool Catalog Page

Brand
Facility Explorer
Document type
Catalog Page
Document number
LIT-1900687
Revision date
2018-06-01
Language
English
Table 1. Handheld VAV Balancing Tool Accessories

Product Code Number

Description

FX-ATV7003-0 Handheld VAV Box Balancing Tool
FX-BTCVTCBL-700 Cable Replacement Set for the FX-BTCVT-1 or the FX-ATV7003-0; Includes One 5 ft (1.5 m) Retractable Cable
FX-ZFRCBL-0 Wire Harness which allows an FX-PCV1610/1620 to be connected to an SA Bus device (Bluetooth® Commissioning Converter, Local Controller Display, or NS Series Sensor) when its SA Bus RJ-12 jack is occupied by an FX-ZFR1811 router.