Network Security Options - Facility Explorer - LIT-12013685 - F4-XPM09090 - F4-XPM18000 - F4-XPM04060 - F4-XPM Expansion Module

F4-XPM Series Protocol Implementation Conformance Statement

Product
Controls > Expansion Modules > F4-XPM Expansion Module
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013685
Revision date
11/11/2020

Non-secure Device - is capable of operating without BACnet Network Security

Secure Device - is capable of using BACnet Network Security (NS-SD BIBB)

 

Multiple Application-Specific Keys:

 

Supports encryption (NS-ED BIBB)

 

Key Server (NS-KS BIBB)