Document Introduction - Facility Explorer - LIT-12013685 - F4-XPM04060 - F4-XPM09090 - F4-XPM18000 - F4-XPM

F4-XPM Series Protocol Implementation Conformance Statement

Brand
Facility Explorer
Product name
F4-XPM
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013685
Revision date
2020-11-11
Language
English

This document contains the Protocol Implementation Conformance Statement (PICS) and BACnet® Interoperability Building Blocks (BIBBs) for the Facility Explorer XPM series input/output expansion modules as required by the ANSI/ASHRAE Standard 135 for BACnet protocol. The PICS is a written document created by the manufacturer of a device to identify the particular options specified in the BACnet standard and implemented in the device. BIBBs are collections of one or more BACnet services. This document includes a listing of the BIBBs currently supported by the XPM04060, XPM09090, and XPM18000.