Character Sets Supported - Facility Explorer - LIT-12013685 - F4-XPM09090 - F4-XPM18000 - F4-XPM04060 - F4-XPM Expansion Module

F4-XPM Series Protocol Implementation Conformance Statement

Product
Controls > Expansion Modules > F4-XPM Expansion Module
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013685
Revision date
11/11/2020

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

IBM®/Microsoft® Double-Byte Character Set (DBCS)

ISO 10646 Universal Character Set-2 (UCS-2)

ISO 10646 (UCS-4)

ISO10646 (UTF-8)

ISO 8859-1

Japanese Industrial Standard (JIS) X 0208