Introduction - Facility Explorer - LIT-12013669 - F4-SNC1612x-0xx - F4-SNC2515x-0xx - Supervisory Device - F4-SNC Supervisory Controller

F4-SNC Product Bulletin

Product
Controls > Supervisory Controls > F4-SNC Supervisory Controller
Document type
Product Bulletin
Document number
LIT-12013669
Revision date
12/12/2022
Product status
Active

The Facility Explorer SNC series (F4-SNC) are Ethernet-based, supervisory controllers that connect Building Automation System (BAS) networks to IP networks.

The SNC perform a key role in the FX system architecture. They provide network management and system-wide control coordination over one or more networks of controllers, including the following devices:

  • CG series general purpose equipment controllers
  • CV series VAV box controllers
  • PCG and PCA programmable controllers
  • PCV series VAV box controllers

These devices monitor and control networks of field-level building automation devices, including HVAC equipment, lighting, security, and fire safety equipment.

In addition to providing supervisory control capabilities, the SNC series also feature onboard input and output interfaces (I/O) and direct digital control capabilities of a controller.

SNC Series

Figure 1. F4-SNC2515x-0
Figure 2. F4-SNC2515x-0H
Figure 3. F4-SNC1612x-0

See Ordering information for SNC models for more information on the model types available.