Features and benefits - Facility Explorer - LIT-1901197 - F4-DLK0350-0 - F4-DLK0350 Local Controller Display
F4-DLK0350 Local Controller Display Catalog Page
- Product
- Controls > Control Displays > F4-DLK0350 Local Controller Display
- Document number
- LIT-1901197
- Revision date
- 2022-07-19
- Product status
- Active
- At-a-glance system status
- Provides quick access to view the current status of monitored points without
logging in.
- Sleek and modern packaging and styling
- Provides a modern, aesthetically pleasing industrial design.
- Local access to operating parameters, setpoints, alarms, and trends
- Provides end users and field technicians the ability to quickly
troubleshoot issues and restore control while being in close proximity to
the associated mechanical equipment.
- Menu-based screen design
- Provides an intuitive user interface through the use of a simple
keypad.
- Tactile keypad
- Provides haptic feedback to the user upon interaction.
- Back-lit LCD
- Provides constant backlight that activates during user interaction to ensure
excellent readability in low-light environments.
- Customized user preferences
- Use to specify settings such as password timeout, backlight intensity, time
and date format, and many more.
- Password protection (Optional)
- Secures the display from unauthorized users.