Mounting the DX-PCA-Adapter - Facility Explorer - Part No. 24-11064-00013 - DX-PCA-Adapter - Field Device - DX-PCA-Adapter

DX-PCA-Adapter Installation Instructions

Product
Accessories > Adapters > DX-PCA-Adapter
Document number
Part No. 24-11064-00013
Document revision
A
Revision date
2019-03-22

About this task

Note: See Wiring prior to mounting the adapter.

Procedure

  1. Remove the existing four corner screws holding the current DX-9100-8900 base unit. Be sure to keep the base unit in its same current position (Figure 1).
  2. Keep the screws for reuse.
  3. Locate the two main pin connectors on the bottom of the adapter (Figure 1) and align them to the connectors of the DX-9100 base unit.
  4. Be sure that the mounting connections of each corner of the metal bracket are aligned correctly with the mounting screws of the corners of the DX base unit when the terminal block sections are lined up. See Figure 1 for a representation of the terminal blocks on the adapter.
    Note: Figure 1 resembles the underside of the adapter.
    Figure 1. Terminal blocks on adapter (underside view)
    Note: The position of the PCA3613 controller on the base adapter may be different than what is shown.
  5. Press the bracket assembly firmly into place. Be sure that all the pins are aligned correctly.
  6. Reinstall the four corner screws. Fasten down the adapter to the base of the DX controller. Do not over-tighten the screws. See Figure 2 Figure 3 .
    Figure 2. Reinstall and tighten screws

    Once the adapter assembly is mounted to the base of the DX controller, the unit should resemble the following photo:

    Figure 3. Adapter mounted to the base of DX Controller

    Note: The position of the PCA3613 controller on the base adapter may be different than what is shown.