Features and benefits - Facility Explorer - LIT-1901144 - DX-ADPT-PCA4911 - Field Device - DX-ADPT-PCA4911 Digital Controller

DX-ADPT-PCA4911 Catalog Page

Product
Controls > Field Controls > DX-ADPT-PCA4911 Digital Controller
Document number
LIT-1901144
Revision date
2020-08-17
Uses existing base of the DX Controller
Allows the footprint mounting location of the replacement FX-PCA4911 to remain the same as the existing DX-9100 Series controller. The addition of a new panel to meet the physical requirements of the FX-PCA4911 may be avoided.
Field Wiring terminated to the base of the DX Controller
Requires minimal re-wiring because the base is reused and is not removed from the panel. The DX-ADPT-PCA4911 comes with most terminations pre-wired and ready to be assembled. Test sites determined that this feature alone could save hours of field labor time for each controller upgrade.
Pre-wired to the FX-PCA4911 Controller
Reduces or eliminates the chance of wire termination errors.