Features and benefits - Facility Explorer - LIT-1901144 - DX-ADPT-PCA4911 - Field Device - DX-ADPT-PCA4911 Digital Controller
DX-ADPT-PCA4911 Catalog Page
- Product
- Controls > Field Controls > DX-ADPT-PCA4911 Digital Controller
- Document type
- Catalog Page
- Document number
- LIT-1901144
- Revision date
- 17/08/2020
- Uses existing base of the DX Controller
- Allows the footprint mounting location of the replacement FX-PCA4911
to remain the same as the existing DX-9100 Series controller.
The addition of a new panel to meet the physical requirements of the FX-PCA4911
may be avoided.
- Field Wiring terminated to the base of the DX Controller
- Requires minimal re-wiring because the base is reused and is not removed from
the panel. The DX-ADPT-PCA4911
comes with most terminations
pre-wired and ready to be assembled. Test sites determined that this feature
alone could save hours of field labor time for each controller upgrade.
- Pre-wired to the FX-PCA4911
Controller
- Reduces or eliminates the chance of wire termination errors.