Network Port - Facility Explorer - LIT-12013127 - FX-PCV1930-0 - FX-PCA4911-0 - Field Device - FX-PCV19 Programmable VAV Box Controller - FX-PCA49 Advanced Application Programmable Controller - FX BACnet/IP Controller

BACnet/IP FX-PCA4911 and FX-PCV1930 Controllers Protocol Implementation Conformance Statement

Product
Variable Air Volume > Variable Air Volume Box Controls > FX-PCV19 Programmable VAV Box Controller
Controls > Programmable Controls > FX-PCA49 Advanced Application Programmable Controller
Controls > Field Controls > FX BACnet/IP Controller
Document number
LIT-12013127
Revision date
2020-11-11

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Network Port

Property Name

Required

Optional

Proprietary

Property ID

Data Type

Writable

Range

APDU_LENGTH X   399 X 128 to 65,535
CHANGES_PENDING X 416
LINK_SPEED X 420
NETWORK_NUMBER X   425 X 0 to 65,534
NETWORK_NUMBER_QUALITY X   426
NETWORK_TYPE X 427
OBJECT_NAME X 77
OUT_OF_SERVICE X 81
PROTOCOL_LEVEL X 482
RELIABILITY X 103
STATUS_FLAGS X 111
BACNET_COMMAND X 417 X
BACNET_MAC_ADDRESS X 423 X
DESCRIPTION X 28 X
BACNET_IP_MODE   X   408      
BACNET_IP_ADDRESS   X   400      
BACNET_IP_UDP_PORT   X   412      
IP_SUBNET_MASK   X   411      
IP_DEFAULT_GATEWAY   X   401      
IP_DNS_SERVER   X   406      
IP_DHCP_ENABLE   X   402      
BBMD_BROADCAST_DISTRIBUTION_TABLE   X   414   X  
BBMD_ACCEPT_FD_REGISTRATIONS   X   413   X  
BBMD_FOREIGN_DEVICE_TABLE   X   415      
ALARM_STATE X 1006 Enumerated
ENABLED X 673 Boolean X
EXECUTION_PRIORITY X 2197 Enumerated X
ITEM_REFERENCE X 32527 Character String
JCI_NPO_APDU_RETRIES X 1851 Byte X 2 to 10
JCI_NPO_APDU_SEGMENT_TIMEOUT X 1849 Unsigned Integer X 1,000 to 65,535
JCI_NPO_APDU_TIMEOUT X 1850 Unsigned Integer X 1,000 to 65,535
JCI_NPO_CHANGES_PENDING_BITSTRING X 1852 Byte
OBJECT_CATEGORY X 908 Enumerated X
PROT_ENG_OUT_RESOURCE X 2020 Unsigned
STATUS X 512 Enumerated
USAGE_TIMEOUT X 2864 Byte
USER_NAME X 2390 Character String