Standard Object Types Supported - Facility Explorer - LIT-12013127 - FX-PCV1930-0 - FX-PCA4911-0 - Field Device - FX-PCV19 Programmable VAV Box Controller - FX-PCA49 Advanced Application Programmable Controller - FX BACnet/IP Controller

BACnet/IP FX-PCA4911 and FX-PCV1930 Controllers Protocol Implementation Conformance Statement

Product
Variable Air Volume > Variable Air Volume Box Controls > FX-PCV19 Programmable VAV Box Controller
Controls > Programmable Controls > FX-PCA49 Advanced Application Programmable Controller
Controls > Field Controls > FX BACnet/IP Controller
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013127
Revision date
2020-11-11

The following is a list of the standard object types as defined by ASHRAE that are currently supported in this product. See the section of the supported object type for details.

  • Accumulator
    Note: The Accumulator object type is only supported in the FX-PCA4911-0 models
  • Analog Input

  • Analog Output

  • Analog Value

  • Binary Input

  • Binary Output

  • Binary Value

  • Calendar

  • Device

  • Event Log

  • File

  • Multistate Value

  • Network Port

  • Notification Class

  • Schedule

  • Trend Log