Document Introduction - Facility Explorer - LIT-12013127 - FX-PCA4911-0 - FX-PCV1930-0 - Field Device - FX BACnet/IP Controller - FX-PCA49 Advanced Application Programmable Controller - FX-PCV19 Programmable VAV Box Controller

BACnet/IP FX-PCA4911 and FX-PCV1930 Controllers Protocol Implementation Conformance Statement

Product
Variable Air Volume > Variable Air Volume Box Controls > FX-PCV19 Programmable VAV Box Controller
Controls > Programmable Controls > FX-PCA49 Advanced Application Programmable Controller
Controls > Field Controls > FX BACnet/IP Controller
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013127
Revision date
2020-11-11

This document contains the Protocol Implementation Conformance Statement (PICS) and BACnet® Interoperability Building Blocks (BIBBs) for the PCA2513 and PCA3613 as required by the ANSI/ASHRAE Standard 135 for BACnet.

The PICS is a written document created by the manufacturer of a device to identify the particular options specified in the BACnet standard and implemented in the device.

BIBBs are collections of one or more BACnet services. This document includes a listing of the BIBBs currently supported by the PCA2513 and PCA3613 .