Character Sets Supported - Facility Explorer - LIT-12013127 - FX-PCV1930-0 - FX-PCA4911-0 - Field Device - FX-PCV19 Programmable VAV Box Controller - FX-PCA49 Advanced Application Programmable Controller - FX BACnet/IP Controller

BACnet/IP FX-PCA4911 and FX-PCV1930 Controllers Protocol Implementation Conformance Statement

Product
Variable Air Volume > Variable Air Volume Box Controls > FX-PCV19 Programmable VAV Box Controller
Controls > Programmable Controls > FX-PCA49 Advanced Application Programmable Controller
Controls > Field Controls > FX BACnet/IP Controller
Document number
LIT-12013127
Revision date
2020-11-11

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

IBM®/Microsoft® Double-Byte Character Set (DBCS)

ISO 10646 Universal Character Set-2 (UCS-2)

ISO 10646 (UCS-4)

ISO10646 (UTF-8)

ISO 8859-1

Japanese Industrial Standard (JIS) X 0208