USB ports and pushbutton switches - Facility Explorer - Part No. 24-10143-861 - Supervisory Device - FX Supervisory Controller

FX80 Supervisory Controller Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10143-861
Document revision
A
Revision date
2019-03-22

Two USB ports, two pushbutton switches, and an associated LED are located behind the controller's front access door.

Figure 1. USB ports and switches behind the access door

Table 1. USB ports and switches

Callout

Description

1

PROG - USB 2.0 to use with USB flash drive for backup

2

DEBUG - Micro-A USB for serial debug communication

3

BACKUP - Pushbutton switch to start a USB backup, or if pressed in during power up/startup, a factory recovery image

4

SHT/DWN - Recessed switch for controlled shutdown

5

BACKUP - LED to indicate USB media present, or a backup, restore, or factory recovery image in progress

The DEBUG port is a standard Micro-A type USB port for serial debug communications to the controller. Use a serial terminal program (for example: PuTTY) to access the controller’s system shell menu. The system shell menu provides access to a few basic platform settings.

The default DEBUG port settings are 115200, 8, N, 1 (baud rate, data bits, parity, stop bits).