Power Up and initial checkout - Facility Explorer - Part No. 24-10143-861 - Supervisory Device - FX Supervisory Controller

FX80 Supervisory Controller Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10143-861
Document revision
A
Revision date
2019-03-22

Procedure

  1. Apply power. To do this, do one of the following:
    • Insert the 2-position 24 V power connector plug.
    • Insert the barrel plug of the wall-mount AC adapter (FX-SC8XPS-0).
  2. Check the STAT (Status) and BEAT (Heartbeat) LEDs.

    When power is applied, the green STAT LED flashes. This LED indicates that the system is working, with power applied. During startup, the BEAT LED may blink at 1 Hz with a 90/10 percent on/off duty cycle. When startup completes, the platform daemon is started, and the normal 1 Hz flash at 50/50 percent on/off duty cycle of the BEAT LED returns.