LEDs - Facility Explorer - Part No. 24-10143-861 - Supervisory Device - FX Supervisory Controller

FX80 Supervisory Controller Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10143-861
Document revision
A
Revision date
2019-03-22

The controller provides a number of status LEDs. All but one of the LEDs are visible with the front access door closed.

Figure 1. LEDs and descriptions

Table 1. LEDs and descriptions

Callout

Description

1

Wi-Fi (Green) - Lit when Wi-Fi configuration switch is not off

2

RS-485 A (COM1) - Transmit (TX) and Receive (RX)

3

RS-485 B (COM2) - Transmit (TX) and Receive (RX)

4

STAT (Green) - Remains lit when controller is powered

5

BEAT (Yellow) - Heartbeat, normally 1 Hz 50% duty cycle

6

Secondary Ethernet - SEC (LAN2) Link and Activity

7

Primary Ethernet - SEC (LAN1) Link and Activity

8

(Behind door) BACKUP (Green) - Typically off

If the BEAT LED stays on constantly, does not light, or blinks very fast, have your ABCS Distributor contact the FSC or your appropriate technical support group.

Important: The 1 Hz, 90/10 percent on/off BEAT flash at startup also occurs during other critical operations, such as a firmware upgrade to the controller or any attached modules. To be safe, do not remove power from the controller while its BEAT LED flashes with a 90/10 percent on/off duty cycle. Wait for the normal (50/50 percent) flash to return before removing power.