Applications - Facility Explorer - Part No. 24-10143-861 - Supervisory Device - FX Supervisory Controller

FX80 Supervisory Controller Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10143-861
Document revision
A
Revision date
2019-03-22
This document describes how to mount and wire the following:
  • DIN-mount, 24 VAC/DC powered FX80 controller
  • Wall-mount, Class 2 universal AC power adapter supplying 24 VAC
Note: The FX80 controller requires, at a minimum, FX Supervisory Release 14.1. A maximum of four total option card modules are supported. Separate limits may exist in the controller’s license to further limit functionality.
Figure 1. FX80 Controller