The controller does not turn on due to one of the
following problems:
- The transformer trips. Power is at the
transformer primary and there is no voltage at the
secondary.
- The breaker or fuse trips. Power is at
transformer primary. There is 24 V at secondary and 0 V at
breaker or fuse.
|
The transformer shorted. |
- Ensure that the polarity of ~24 V COM, +15 V COM, and SA BUS
COM on the controller, auxiliary devices, and input and
output devices is the same.
- Verify that the short circuit has been resolved with an
ohm-meter.
- Reset the breaker or fuse, or replace the transformer.
Note: When you replace
the transformer, replace it with a model that uses a
resettable circuit breaker. A circuit breaker makes it
easier to solve wiring problems.
- To verify the connection, complete the following steps:
- Disconnect the secondary of the 24 VAC
transformer.
- Use an ohm-meter to measure between ~24 V H and G at
the controller. Ensure that no short circuit
occurs.
Note: If your
installation requires that you earth ground the
transformer secondary, verify that the earth
ground connection is valid and not shared between
multiple pieces of equipment.
|
The 24 VAC powered sensor is not wired with the same polarity as
the controller. |
The SA Bus device is not wired with the same polarity as the
controller. |
Analog output mode is invalid. 0 V to 10 V output is set to 100%,
but output terminals are less than 10 V. |
Load impedance is lower than 5K ohms. |
- Ensure that the voltage control device load impedance is
higher than 5,000 ohms. For more information, refer to
voltage device manufacturer specification.
- Disconnect the connected device and verify that the value
you require is present.
|
Analog mode for a configurable output is invalid. For example, 0
V to 10 V output has an undesirable offset of up to 1 V. |
The COM terminal is not connected. |
- Connect the COM terminal of the configurable output to the
common of the connected end device.
- Measure the output and verify that it matches the
command.
- Disconnect the connected device and verify the commanded
value is present.
|
The Common Reference is incorrect. |