Connecting to a controller with Wi-Fi - EasyIO - LIT-12013983 - Building Management - FW-VAV Variable Air Volume Controller

FW-VAV Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12013983
Document revision
0
Revision date
2023-08-16

Procedure

  1. From the desktop toolbar on your computer, click your Wi-Fi network icon.
  2. Find the controller's SSID, then connect to the controller.
    Note: Your controller's default SSID is a combination of the controller's series letters and the last four characters of the controller's MAC address, for example, FW-012A. You can find the MAC address on the label on the back of the controller.
  3. Enter the default password. For more information, contact your supplier.
  4. At the command line, enter ping followed by the controller's IP address to ping the controller
    Note: For more information about your controller's default IP address, see Primary network default IP address, subnet mask, and gateway.