Controller interfacing - EasyIO - LIT-12013983 - Building Management - FW-VAV Variable Air Volume Controller

FW-VAV Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12013983
Document revision
0
Revision date
2023-08-16

To interface with a controller and its inputs and outputs with CPT and the controller's web server, establish a connection from your device. You can connect to your controller with a device through Ethernet or though Wi-Fi.

Note: Use the following procedures to set up a controller on a primary network. For more information about a secondary network setup, refer to the product's User Reference Guide.

Interface with your controller with the following user interfaces: