The controller does not turn on due to one of the following
problems:
- The transformer trips. Power is at the
transformer primary and there is no voltage at the
secondary.
- The breaker or fuse trips. Power is at
transformer primary and there is 24 V at secondary and 0 V at
breaker or fuse.
|
The transformer shorted. |
- Ensure that the polarity of ~24 V COM, +15 V
COM, and SA BUS COM on the controller, auxiliary devices, and
input and output devices is the same.
- Verify that the short circuit is resolved with an ohm-meter.
- Reset the breaker or fuse, or replace the transformer.
Note: If you replace the
transformer, replace it with a model that uses a resettable
circuit breaker. A circuit breaker makes it easier to solve
wiring problems.
- To verify the connection, complete the
following steps:
- Disconnect the secondary of the 24 VAC transformer.
- Use an ohm-meter to measure between ~24 V at terminal H and G at the
controller. Ensure that no short circuit occurs.
Note: If your
installation requires that you earth ground the
transformer secondary, verify that the earth ground
connection is valid and not shared between multiple
pieces of equipment.
|
| The 24 VAC powered sensor is not wired with the same
polarity as the controller. |
| The SA bus device is not wired with the same polarity as the
controller. |
| Analog output mode is invalid. 0 V to 10 V output is
set to 100%, but output terminals are less than 10 V. |
Load impedence is lower than 5,000 ohms. |
- Ensure that the voltage control device load impedance is higher than
2,000 ohms. For more information, refer to voltage device
manufacturer specification.
- Disconnect the connected device and verify that
the value you require is present.
|
| Analog mode for a configurable output is invalid. For example, 0 V to
10 V outputs an unwanted offset of up to 1 V. |
The COM terminal is not
connected. |
- Connect the COM terminal of the configurable
output to the common of the connected end device.
- Measure the output and verify that it matches
the command.
- Disconnect the connected device and verify the
commanded value is present.
|
| The Common Reference is incorrect. |