Removing the controller cover - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

About this task

Remove the controller cover to access the circuitry, jumpers, and to better access the reset and service buttons.

Procedure

  1. Use a Philips screwdriver to unscrew both of the top cover screws.
    Figure 1. Unscrewing the cover
  2. Hold both ends of the top cover and remove it. If the top cover is stuck, separate the cover with a slotted screwdriver.
    Figure 2. Removing the cover