The FW-08V is an input/output controller with IP network, Ethernet, MS/TP, and
Wi-Fi connectivity. Use this guide to learn more about the following topics:
- Understanding the controller components
- Mounting the controller on a DIN rail or enclosure base plate
- Installing the antennas
- Viewing a wiring diagram of the controller in a system
- Connecting to the controller with a LAN or Wi-Fi connection
- Connecting to the controller with the Controller programming tool (CPT) application
- Connecting to the controller's web server dashboard with CPT graphics
Figure 1. FW-08V, front
Figure 2. FW-08V, back and side
Callout | Description | |||
---|---|---|---|---|
1 | DIN rail | |||
2 | Enclosure mount | |||
3 | Cover screw | |||
4 | H and G terminal | |||
5 | Universal output (UO) and COM terminals | |||
6 | LED indicators | PWR | Power LED | |
ERR | Error LED | |||
STS | Status LED | |||
TXRX | Transmitting or receiving communication LED | |||
For more information about LED states, see FW LED states | ||||
RST | Reset button. For more information on how to reset the controller, refer to FW Series Commissioning Guide. | |||
SVC | Service button | |||
7 | RP-SMA female antenna jacks | |||
8 | RS485 serial port terminals | |||
9 | Antennas | |||
10 | Ethernet ports | |||
11 | Differential pressure flow sensor | |||
12 | Universal input (UI) and COM terminals | |||
13 | Mounting clips |