Mounting the controller to the enclosure base plate - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 point variable air volume controller - 1.0

FW-08V Quick Start Guide

Brand
EasyIO
Product name
EasyIO FW-08V series 8 point variable air volume controller
Document type
Quick Start Guide
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active
Language
English

If a DIN rail mount is not practical, the controller features two mounting holes to screw mount the controller to an enclosure base plate. See Figure 1 for the mounting hole locations on the controller.