Installing the antennas - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

Procedure

  1. Locate the two RP-SMA female jacks. See overview.
  2. To connect the male antenna connectors to the female RP-SMA jacks, screw on the antennas in a clockwise direction.
    Note: For a secure connection, when you tighten the antennas to the female RP-SMA jack, hold the metal part of the RP-SMA male connector. A poor connection can affect reception.
    Figure 1. Screwing on the antennas
  3. Adjust the direction of the antennas to find the best reception.