Universal input jumper configuration - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

The FW-08V controller supports resistance and voltage field devices. For resistance mode, position the jumper on the two left pins. For voltage mode, position the jumper on the two right pins.

Note: You can configure each UI individually.
Figure 1. Resistance mode
Figure 2. Voltage mode