FW LED states - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

The following table displays the LEDs blink rate descriptions:

Table 1. FW LED states
LED label LED colour Normal state State Description
ERR Red Off steady Constant rapid blinks A communication error is present between the FM-02 module and the base board.
On steady Firmware upgrade in process. Ensure that there is no power loss during this period.
Off steady No errors
STS Green 1 Hz blinks

1 Hz blinks

Normal operation
Off steady A controller fault is present
TXRX Yellow 1 Hz to 5 Hz blinks 1 Hz to 5 Hz blinks Normal data communication

Off steady

No data transmission