Interfacing with controller objects using CPT - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

Use CPT to program FW-08V controller logic with the Sedona framework.

Procedure

  1. To download the CPT application, contact Support for the latest release.
  2. Unzip the folder and double-click the cpt.exe file.
    Important: If the CPT application is already installed on your computer and you want to update it to a new release, do not click and launch the cpt.exe file to avoid personal settings data loss. Unzip the package and drop all the files into the existing CPT folder to merge and overwrite outdated files.
  3. To connect to a controller, click File, click Open App.
  4. In the Project Management window, on the Recent tab, click New.
  5. In the App Desc field, enter a name for the controller.
  6. In the Host field, enter the controller's IP address.
    Note: The default IP address is 192.168.10.30.
    Note: For more information about your controller's IP address, refer to the Controller series IP address, subnet mask, and data folder section of the CPT User Guide (LIT-12013978).
  7. From the Data Folder list, select the folder for your controller type.
    Note: For more information about your controller's data folder, refer to the Controller series IP address, subnet mask, and data folder section of the CPT User Guide (LIT-12013978).
  8. Click Save.
  9. Click Open.
  10. In the Authentication dialog, enter your password in the Password field.
    Note: By default, there is no password. To increase security, when you log on, complete the steps in Creating a new CPT admin password for a controller in EasyIO Hardening Guide (LIT-12013986) .

What to do next

For more information about CPT, Refer to the CPT User Guide (LIT-12013978).