Interfacing with a controller's web server - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

About this task

To interface with a controller's web server, complete the following steps:

Procedure

  1. Launch a HTML5 web browser, such as Chrome™, Firefox®, Microsoft Edge®, or Safari®.
  2. In the web browser's address bar, enter your controller's IP address, then press the Enter key or Return key.