Connecting to a controller with Wi-Fi - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

Procedure

  1. From the desktop toolbar on your computer, click your Wi-Fi network icon.
  2. Find the controller's SSID, then connect to the controller.
    Note: Your controller's default SSID is a combination of the controller's series letters and the last four characters of the controller's MAC address, for example, FW-012A. You can find the MAC address on the label on the back of the controller.
  3. Enter the default password. For more information, contact your supplier.
  4. At the command line, enter ping followed by the controller's IP address to ping the controller
    Note: For more information about your controller's default IP address, see Primary network default IP address, subnet mask, and gateway.