Connecting a controller with an Ethernet cable - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

Procedure

  1. Connect your computer to the controller with an Ethernet cable.
  2. Set up your network adapter in the same range as the controller. To change your IP address, subnet mask, and gateway, complete the steps as outlined in one of the following options, depending on your operating system:
    Note: Use the same subnet mask and gateway as the controller. For the IP address, enter the same IP address as the controller, but change the last octet to a unique number. Use a high number that is less than 255 to avoid using an IP address that is already in use. For more information about your controller's IP address, subnet mask, and gateway, see Primary network default IP address, subnet mask, and gateway.