Controller interfacing - EasyIO - LIT-12014189 - Building Management - EasyIO FW-08V series 8 Point Variable Air Volume Controller - 1.0

FW-08V Quick Start Guide

Product
Document number
LIT-12014189
Version
1.0
Revision date
2023-08-25
Product status
Active

To interface with a controller and its inputs and outputs with CPT and the controller's web server, establish a connection from your device. You can connect to your controller with a device with the following options:

Note: Use the following procedures to set up a controller on a primary network. For more information about a secondary network setup, refer to the product's User Reference Guide.

Interface with your controller with the following user interfaces: