Power supply terminal wiring - EasyIO - LIT-12014308 - EASYIO-FT-04B - Building Management - EasyIO FT-04B 4 Point Controller

FT-04B Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12014308
Document revision
1.0
Revision date
2023-07-27
Product status
Active

Connect the 24 VAC supply power wires from the transformer to the HOT and COM power terminals as shown in Figure 1.

Note: The supply power wire colors may differ on transformers from other manufacturers. Refer to the transformer manufacturer’s instructions and the project installation drawings for wiring details.
Important: To reduce noise, interference, and ground loop problems, connect a 24 VAC supply power to the controller and to all other network devices so that transformer phasing is uniform across network devices. The controller does not require an earth ground connection. However, when you need to ground the secondary of the 24 VAC transformer, make only one ground connection near the transformer. For more information, see the following figure.
Figure 1. Transformer grounding
CAUTION
  • To avoid property damage, check all wiring connections before you apply power to the system. If you wire this terminal incorrectly, a short circuit can occur across the 24 VAC power supply on the controller. A short circuit can cause a tripped circuit breaker or a blown fuse. If you use a transformer with a built-in fuse, you may need to replace the transformer.