Procedure
- On the desktop toolbar on your computer, click your Wi-Fi network icon.
-
Find the controller's SSID, then connect to the
controller.
Note: Your controller's default SSID is a combination of the controller's series letters and the last four characters of the controller's MAC address, for example, FT-012A. You can find the MAC address on the label on the back of the controller.
- Enter the default password. For more information, contact your supplier.
-
To ping the controller, at the command line, enter
ping, followed by the controller's IP address.Note: For more information on your controller's default IP address, see Primary network default IP address, subnet mask, and gateway.