Troubleshooting - EasyIO - LIT-12014187 - EASYIO-FT-04A - EasyIO FT-04A 4 Point Controller - EasyIO FT-04B 4 Point Controller

FT-04A Quick Start Guide

Product
Document number
LIT-12014187
Document revision
1.0
Revision date
2023-07-27
Product status
Active
Table 1. Troubleshooting
Problem Cause Solution
The controller does not turn on due to one of the following problems:
  • The transformer trips. Power is at the transformer primary and there is no voltage at the secondary.
  • The breaker or fuse trips. Power is at transformer primary. You find 24 V at secondary and 0 V at breaker or fuse.
The transformer shorted.
  1. Ensure that the polarity of ~24 V COM on the controller, auxiliary devices, and input and output devices is the same.
  2. Verify that the short circuit is resolved with an ohm-meter.
  3. Reset the breaker or fuse, or replace the transformer.
    Note: If you replace the transformer, replace it with a model that uses a resettable circuit breaker. A circuit breaker makes it easier to solve wiring problems.
  4. To verify the connection, complete the following steps:
    1. Disconnect the secondary of the 24 VAC transformer.
    2. Use an ohm-meter to measure between ~24 V H and G at the controller. Ensure that no short circuit occurs.
      Note: If your installation requires that you earth ground the transformer secondary, verify that the earth ground connection is valid and not shared between multiple pieces of equipment.
The 24 VAC powered sensor is not wired with the same polarity as the controller.
Analog output mode is invalid. 0 V to 10 V output is set to 100%, but output terminals are less than 10 V. Load impedance is lower than 2k ohms.
  1. Ensure that the voltage control device load impedance is higher than 2k ohms. For more information, refer to voltage device manufacturer specification.
  2. Disconnect the connected device and verify that the value you require is present.
Analog mode for a configurable output is invalid. For example, 0 V to 10 V output results in an unwanted offset of up to 1 V. The COM terminal is not connected.
  1. Connect the COM terminal of the configurable output to the common of the connected end device.
  2. Measure the output and verify that it matches the command.
  3. Disconnect the connected device and verify the commanded value is present.
The Common Reference is incorrect.