Controller interfacing - EasyIO - LIT-12014187 - EASYIO-FT-04A - EasyIO FT-04A 4 Point Controller - EasyIO FT-04B 4 Point Controller

FT-04A Quick Start Guide

Product
Document number
LIT-12014187
Document revision
1.0
Revision date
2023-07-27
Product status
Active

To interface with a controller and its inputs and outputs with Controller Programming Tools (CPT) and the controller's web server, establish a connection from your device.

Note: Use the following procedures to set up a controller on a primary network. For more information about a secondary network setup, refer to the product's User Reference Guide.