Use CPT to program EasyIO controller logic with the Sedona framework.
Procedure
- To download the CPT application, contact Support for the latest release.
-
Unzip the folder and double-click the
cpt.exefile.Note: If CPT is already installed on your computer and you want to update it to a new release, do not click and launch thecpt.exefile to avoid personal settings data loss. Instead, unzip the package and drop all the files into the existing CPT folder to merge and overwrite outdated files. - To connect to a controller, click File, then click Open App.
- In the Project Management window, on the Recent tab, click New.
- In the App Desc field, enter a name for the controller.
-
In the Host field, enter the controller's IP
address.
Note: The default IP address is 192.168.4.1Note: For more information about your controller's IP address, refer to the Controller series IP address, subnet mask, and data folder section of the EasyIO CPT User Guide (LIT-12013978).
-
From the Data Folder list, select the folder for your controller type.
Note: For FS Series controllers, select SedonaFG.Note: For more information about your controller's data folder, refer to the Controller series IP address, subnet mask, and data folder section of the EasyIO CPT User Guide (LIT-12013978).
- Click Save.
- Click Open.
-
In the Authentication
dialog, enter your password in the Password field.
Note: By default, there is no password. To increase security, when you log on, complete the steps in Creating a new CPT admin password for a controller in EasyIO Hardening Guide (LIT-12013986).