Compliance - EasyIO - LIT-12014187 - EASYIO-FT-04A - EasyIO FT-04A 4 Point Controller - EasyIO FT-04B 4 Point Controller

FT-04A Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12014187
Document revision
1.0
Revision date
2023-07-27
Product status
Active
Table 1. FT-04A Compliance
North America: UL 916 Energy Management Equipment;

FCC Class B, Part 15, Subpart C 15.247

FCC

This device contains licence-exempt transmitter(s)/receiver(s) that comply with Innovation, Science and Economic Development Canada’s licence-exempt RSS(s). This device complies with part 15 of the FCC Rules.

Operation is subject to the follow-ing two conditions:

(1) This device may not cause interference.

(2) This device must accept any interference, including interference that may cause undesired operation of the device.

L’émetteur/récepteur exempt de licence contenu dans le présent appareil est conforme aux CNR d’Innovation, Sciences et Développement économique Canada applicables aux appareils radio exempts de licence. L’exploitation est autorisée aux deux conditions suivantes :

1) L’appareil ne doit pas produire de brouillage;

2) L’appareil doit accepter tout brouillage radioélectrique subi, même si le brouillage est susceptible d’en compromettre le fonctionnement.

NOTE: This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential instal-lation. This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interfer-ence will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:

— Reorient or relocate the receiving antenna.

— Increase the separation between the equipment and receiver.

— Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.

— Consult the dealer or an experienced radio/TV technician for help. Limited by local law regulations, version for North America does not have region selection option.

This radio transmitter IC: 2AKZUFT has been approved by Innovation, Science and Economic Development Canada to operate with the antenna types listed below, with the maximum permissible gain indicated. Antenna types not included in this list that have a gain greater than the maximum gain indicated for any type listed are strictly prohibited for use with this device.

Gain of antenna: 2.2 dBi max

Type of antenna: Onboard antenna

Le présent émetteur radio IC: 2AKZUFT a été approuvé par Innovation, Sciences et Développement économique Canada pour fonctionner avec les types d'antenne énumérés ci-dessous et ayant un gain admissible maximal. Les types d'antenne non inclus dans cette liste, et dont le gain est supérieur au gain maximal indiqué pour tout type figurant sur la liste, sont strictement interdits pour l'exploitation de l'émetteur.

Gain d'antenne: 2.2 dBi maximal

Type d'antenne: Antenne embarquée

To satisfy FCC & IC RF exposure requirements, a separation distance of 20 cm or more should be maintained between the antenna of this device and persons during device operation. To ensure compliance, operations at closer than this distance is not recommended. Les antennes installées doivent être situées de facon à ce que la population ne puisse y être exposée à une distance de moin de 20 cm. Installer les antennes de facon à ce que le personnel ne puisse approcher à 20 cm ou moins de la position centrale de l’ antenne.

CE Compliant

RED directive

The Equipment named above is confirmed to comply with the requirements set out in the European Council Directive on the Approximation of the Laws of the Member States relating to 2014/53/EU (RED). The equipment passed the following test which was performed according to the following European standards:

EN 301 489-1 V2.2.0 (2017-03, EN 301 489-17 V3.2.0(2017-03, EN 300 328 V2.1.1(2016-11, EN 62311(2008)

UKCA

Directive Electromagnetic Compatibility Regulations 2016:

BS EN 55032:2015+A11:2020, BS EN IEC 61000-3-2:2019/A1:2021, BS EN 61000-3-3:2013+A1:2019, BS EN 55035:2017+A11:2020