Removing the controller cover - EasyIO - LIT-12014270 - EASYIO-FC-20 - EasyIO FC-20 Controller

FC-20 Quick Start Guide

Product
Controls > Input/Output Controls > EasyIO FC-20 Controller
Document type
Quick Start Guide
Document number
LIT-12014270
Document revision
1.0
Revision date
2024-02-14
Product status
Active

Procedure

  1. Use a Philips screwdriver to unscrew both of the cover screws.
  2. Hold both ends of the cover and remove it. If the cover is stuck, separate the cover from the base with a flathead screwdriver.