About this task
If a DIN rail mount is not practical, the controller features two mounting holes to screw mount the controller to an enclosure base plate.
Procedure
- Place the controller on the enclosure surface and mark the enclosure mounting holes on the surface. For more information, see Enclosure mounting holes in Figure 1.
- Drill both holes in the enclosure base plate.
- Screw the controller to the enclosure base plate.