The FC-20 controller supports resistance, voltage and current field devices. For
resistance mode, position the jumper on the two left pins. For voltage mode, position
the jumper on the two center pins. For current mode, position the jumper on the two
right pins.
Note: You can configure each universal
input individually.
Figure 1. Resistance mode
Figure 2. Voltage mode
Figure 3. Current mode