BACnet or Modbus selection and ID setting - EasyIO - LIT-12014270 - EASYIO-FC-20 - EasyIO FC-20 Controller

FC-20 Quick Start Guide

Brand
EasyIO
Product name
EasyIO FC-20 Controller
Document type
Quick Start Guide
Document number
LIT-12014270
Document revision
1.0
Revision date
2024-02-14
Product status
Active
Language
English

Use the dual in-line package (DIP) switch to select the BACnet or the Modbus protocol. By default, the Modbus protocol is selected. To switch to BACnet, toggle switch 1 upwards to the on position.

Use the switches 2 to 8 to set the BACnet MSTP ID when the switch 1 is on or the Modbus Serial ID when the switch 1 is off. Each of the switches 2 to 8 stand for a binary bit. Toggle the switches upwards to the on position to make that address digit 1 or leave it in the off position to make that address digit 0. The most significant bit (MSB) is DIP 2 and the least significant bit (LSB) is DIP 8.

Table 1.
DIP switch number Function
1 Protocol selection
2 ID 64
3 ID 32
4 ID 16
5 ID 8
6 ID 4
7 ID 2
8 ID 1