The following table displays the FC LED states:
LED label | LED color | Normal state | State | Description |
---|---|---|---|---|
PWR | Green | On steady | Off steady | No power |
On steady | Power is supplied by primary voltage | |||
ERR | Red | Off steady | Constant rapid blinks | RS-485 communication error |
Off steady | No errors | |||
STS | Green | 1 Hz blinks |
1 Hz blinks |
Normal operation |
Off steady | Controller fault | |||
TXRX | Yellow | 1 Hz to 5 Hz blinks | 1 Hz to 5 Hz blinks | Normal data communication |
Off steady |
No data transmission |