VAV features and sequence of operation - EasyIO - LIT-12014127 - EASYIO-FW-VAV - FV-VAV - 1.0

EasyIO FW-VAV Application Note

Brand
EasyIO
Product name
FV-VAV
Document type
Application Note
Document number
LIT-12014127
Version
1.0
Revision date
2024-04-09
Product status
Active
Language
English

The applications control the integrated actuator to adjust the supply air damper. Some applications also include functions to control a box reheat option or different types of fans, if available.