Restoring the default applications - EasyIO - LIT-12014127 - EASYIO-FW-VAV - FV-VAV - 1.0

EasyIO FW-VAV Application Note

Brand
EasyIO
Product name
FV-VAV
Document type
Application Note
Document number
LIT-12014127
Version
1.0
Revision date
2024-04-09
Product status
Active
Language
English

About this task

The FW-VAV contains two backups stored in its flash memory as part of its firmware, the metric units backup and the imperial units backup. You cannot delete or edit these backups. The backups are used to restore the default set of applications into the controller in case an error occurs while you program or edit the applications.

The metric units application is the default application. If you need the imperial units application, you can restore that backup through a web browser.

To restore any of the default backups, complete the following steps:

Procedure

  1. Launch any web browser.
  2. Type in the FW-VAV IP address. The default IP address is 192.168.10.30.
  3. At the bottom left of the browser window, click the + icon to expand the navigation tree.
  4. Click Restore to display a pop-up window.
  5. In the pop up window, click Restore on the backup application you require.