Application overview - EasyIO - LIT-12014127 - EASYIO-FW-VAV - FV-VAV - 1.0

EasyIO FW-VAV Application Note

Brand
EasyIO
Product name
FV-VAV
Document type
Application Note
Document number
LIT-12014127
Version
1.0
Revision date
2024-04-09
Product status
Active
Language
English

You can configure the preloaded FW-VAV controller application to meet any of the six modes listed in Table 1.

The default values for the preloaded applications are in degrees Celsius for the temperature and in liters per second for the flow rate. If you prefer other units such as degrees Fahrenheit and cubic feet, refer to Restoring the default applications for instructions.

Table 1. Preloaded applications
Application name Description
Cooling only Single duct, cooling only, pressure independent
Cooling with 2-stage electric heating Electrical heater with one or two stages, pressure independent
Cooling with modulating heating valve Hot water heating, pressure independent
Cooling and heating with series fan Series fan powered cooling and heating, pressure independent

Cooling with parallel fan powered heating

Cooling with fan powered heating, pressure independent
Variable Air Volume and Temperature (VVT) zone damper Variable volume terminal zone damper, pressure independent, with or without fan